Free chlorine measurement for monitoring water disinfection
Trustable analysis panels for drinking water
Each year, the Basse-Vigneulles plant produces more than 2.3 million m3 of drinking water. The water is taken from the ground water and undergoes the conventional treatment stages: removal of carbon and iron, filtration and disinfection. At the end of the process, the water is disinfected by injecting gaseous chlorine. To optimize the chlorine dosage the plant is equipped with an Endress+Hauser disinfection panel.
The Syndicat des Eaux de Basse-Vigneulles et Faulquemont based in Moselle, France
Analysis panels for drinking water disinfection monitoring
Results
Time saving set-up
Pre-installed panel solution ready to use
Reliable measured values allow precise dosing of chlorine
After several years of operation, we are very pleased with the Endress+Hauser analysis panels measuring the
free chlorine and enable us to monitor the disinfection of the potable water in real time.
Thierry Illy, Water treatment Units Manager
The Syndicat des Eaux de Basse-Vigneulles et Faulquemont
Background
Drinking water reservoir at Redlach
The production of drinking water comprises several treatment steps and is important for safeguarding the health of consumers. Each year, the Basse-Vigneulles plant ensures a continuous flow of drinking water for consumers in 70 communes. Amongst the treatment steps, disinfection is a key part for safe distribution of potable water. Correct dosing the chlorine is a vital parameter in providing high quality water.
Our solution
Disinfection panel at Syndicat des Eaux de Basse-Vigneulles et Faulquemont
To monitor the dosing of the chlorine precisely, the water authority has installed several drinking water analysis panels equipped with Memosens CCS51D sensors for measuring free chlorine. These sensors continuously monitor the proportion of chlorine present in the water. Measurements are taken when the water leaves the production plant, and at the Redlach drinking water reservoir and the distribution network, thereby ensuring that the residual effect of the disinfectant continues.
Vizet, italokat, tejtermékeket, vegyszereket vagy gyógyszereket naponta elemezni kell. Válassza ki az Ön igényeinek leginkább megfelelő készüléket átfogó termékportfóliónkból.
Endress+Hauser is dedicated to helping you meet your operating targets throughout the water cycle by combining an innovative portfolio of measuring instruments, expert services and industry expertise.
Az adatvédelem nagyon fontos számunkra
Sütiket használunk a böngészési élmény javítására, statisztikai adatok gyűjtésére a webhely működésének optimalizálása érdekében, valamint személyre szabott hirdetések vagy tartalmak közvetítésére.
Ha az „Összes elfogadása” lehetőségre kattint, Ön hozzájárul a sütik használatához.
További részletekért kérjük, tekintse meg a sütikre (cookie) vonatkozó irányelveinket .