Title

Próbáljon kulcsszavak, rendelési- vagy termékkód, vagy gyári szám szerint keresni, pl. „CM442” vagy „Műszaki információk”
A keresés elindításához írjon be legalább 2 karaktert.
  • Előzmények

Cement decarbonization: CEMS & analytics for low-carbon clinker

Explore the operational challenges behind cement decarbonization and learn how advanced instrumentation improves process stability, performance and compliance.

Cement plant with rotary kiln, preheater tower and smokestacks emitting flue gas
Introduction

Cement decarbonization: From process emissions to traceable gas analysis

Cement decarbonization relies on reducing CO₂ released during calcination and fuel combustion in the kiln and calciner. These process steps generate most of the plant’s emissions, making reliable measurement critical. A Continuous Emission Monitoring System (CEMS) provides continuous CO₂ and pollutant data, forming the basis of decarbonization and regulatory compliance.

This page explains the technical constraints of cement decarbonization and defines what low‑carbon clinker means from a process perspective. We also outline how continuous gas analysis supports emissions reporting, operational stability and long‑term CO₂ reduction.

Low clinker cement block with green plant symbolizing sustainable and low carbon production ©Adobe Stock/penyushkin
Insights

Low‑carbon clinker: Definition and measurable process criteria

Clinker production is the primary driver of a cement plant’s Scope 1 emissions. Lowering CO₂ emissions requires changes in clinker chemistry, kiln operation or combustion behavior. In addition, material strategies such as reduced limestone content or the use of supplementary materials can reduce CO₂ intensity at the product level.

Low‑carbon clinker refers to clinker with a reduced CO₂ emission factor. From a process perspective, it is defined by three quantifiable elements:

  • Lower calcination emissions per tonne of clinker
  • Reduced fuel-related CO₂
  • CO₂ streams suitable for carbon capture technologies

Each element is addressed in the following sections.

Lower calcination emissions per tonne of clinker

While CO₂ emissions from calcination are chemically unavoidable, overall emissions can be reduced through:

  • Improved kiln and calciner heat efficiency, avoiding overfiring for the required degree of calcination
  • Optimized raw meal chemistry and the use of mineralizers to lower the thermal demand
  • Partial substitution of limestone with materials requiring less decarbonation

These measures reduce the specific CO₂ released from CaCO₃ decomposition, even though the chemical reaction itself cannot be eliminated.

Cement plant complex with silos, rotary kiln and preheater tower in mountainous landscape ©Adobe Stock/Washburn

Reduced fuel-related CO₂

Fuel-related emissions depend on the carbon content of the heat source and the stability of combustion.

Key pathways include:

  • Higher substitution of fossil fuels with alternative fuels such as biogenic fuels and waste-derived fuels (e.g. Refuse-Derived Fuel also known as RDF)
  • Maintaining stable O₂/CO behavior to avoid incomplete combustion
  • Reducing excess air to limit thermal losses
  • Improving calciner efficiency to minimize overall fuel demand

The use of alternative fuels increases variability in combustion, which requires reliable process monitoring and gas analysis to maintain performance and emissions control. A low‑carbon clinker line achieves the same degree of sintering with lower fossil carbon input.

CO₂ streams suitable for carbon capture technologies

Carbon Capture, Utilization and Storage (CCUS) implementation of a clinker process could define an operation as low-carbon in regulatory and market contexts. Before implementation, the operation requires control of the following process parameters:

  • Stable and predictable CO₂ concentration in the preheater or calciner exhaust
  • Low levels of contaminants such as SO₂, HCl and particulates that affect capture efficiency
  • Reliable CEMS data to verify capture performance and reporting accuracy

Plants that deliver a consistent and well-characterized CO₂ exhaust profile are better positioned for future carbon capture integration.

Implementing these decarbonization strategies introduces operational constraints. Alternative fuels can increase combustion variability, while carbon capture requires stable exhaust gas conditions. Plants must therefore balance emission reduction objectives with process stability, clinker quality and production performance. Reliable emissions monitoring is essential to support this transition.

How CEMS anchor compliance strategies in cement plant emissions monitoring ©Adobe Stock/bilanol
Insights

How CEMS supports your compliance strategy

Cement plants must comply with strict environmental and reporting requirements that define what must be measured and how results must be documented. Traceable data is essential for daily operation, regulatory compliance and long-term decarbonization planning.

What must be reported:

  • Scope 1 CO₂ from calcination and fuel combustion
  • Specific CO₂ per tonne of clinker
  • Emission factors for fuels
  • Annual CO₂ totals based on mass balance and CEMS data

Only verified datasets are accepted.

Why CEMS is essential

Certified CEMS provides the continuous emissions data required for reporting and regulatory compliance. It ensures:

  • Reliable and traceable measurements
  • Compliance with standards such as EN 14181 or MCERTS
  • Continuous monitoring of regulated pollutants
  • Audit-ready data

Without valid CEMS data, plants risk non-compliance and emissions recalculation.

How measurement enables carbon capture readiness

Carbon capture projects require stable and verifiable process gas data. This depends on:

  • Stable CO₂ concentration
  • Low contaminant levels
  • Continuous and traceable measurement
Securing business value in cement decarbonization through efficient clinker production
Insights

Securing the business value of your cement decarbonization

When CO₂, O₂, CO, NOx, SO₂ and HCl data is measured reliably throughout the kiln and calciner system, emission control and fuel use become easier to stabilize. This enables the following improvements:

  • Ensure compliance, support Environment Safety and Governance (ESG) and decarbonization targets with continuous and traceable emissions data
  • Optimize fuel consumption through stable O₂ and CO behavior that supports efficient combustion and avoids over‑firing
  • Stabilize clinker quality as gas trends reveal combustion deviations early and allow timely correction
  • Minimize operating and maintenance effort through consistent CEMS performance that reduces troubleshooting and manual verification
FAQ

Frequently asked questions on cement decarbonization with CEMS

This section covers key questions on cement decarbonization, emissions monitoring and process control. It explains the role of CEMS, real-time emission analytics and alternative fuel combustion in maintaining compliance and improving plant performance.

Végjegyzetek